This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM1808 Silicon Errata : DVDD18 Can Pull Up to 2.7V When Using Dual-Voltage IOs at 3.3V

Other Parts Discussed in Thread: TPS65023, AM1808

3377.AM1808 Schematics.docWe are using TPS65023 PMIC to power an AM1808  processor. On some of the boards, the 1.8V (DDR Power) rail is acting strangely. It measures upto 2.7V. We have tried out the workaround in AM1808 silicon errata. But still the issue exists. 

As per the workaround we have 44.9uF bulk capacitance. We have increased the load upto 90uF. But still we have issues in the 1.8V and 3.3V supply. Schematics attached.

Please advice.