Webench Design
Vin = 22 to 26 V
Vout = 5.0 V
Iout = 0.5A max, 0.3 typical.
Note in datasheet(page 11): Use caution when using only ceramic capacitors for input bypassing, because it may cause severe ringing at the VIN pin.
Customer is very concerned about input ripple, EMI and supply stability issues. Using Webench, only ceramic caps are selected for the design which seems to contradict the note in the datasheet.
Question: Will this design be stable with chosen ceramic capacitors ? or is there an issue with Webench ?