Hi All,
TPS65232 is not recommended for new designs by TI.
Could you place advice a replacement part for TPS65232.
Best Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
You may want to look into:
TPS65251 : PMU with 3 DC/DC Converters, up to 18Vin
TPS652510: Three DC-DC Converters with Integrated FET with 4.5V to 16V Input
Hi Gregory,
Thank you for your answers.
Is there any device similar with TPS65232 topology. (One external sync. switch with high current capability, others internal switch..)
Or when TPS65232 device will be obsolete. Because TI new EVM board still using this device. (etc. DM818x )
Best regards.