Other Parts Discussed in Thread: UCD90124A
I use a UCD90124A sequencer with firmware 2.4.0.
I make a RESETn output from several POWER_GOOD outputs and one GPI (pin 18).
Sometimes the RESETn output goes unwanted low and goes mostly never high. Sometimes the RESETn line goes high after +/- 25 ms. But there are no POWER or GPI fault logged.
When I remove the GPI dependence, the RESETn line works fine. I make the conclusion the problem is the GPI input.
I monitor the input with a oscilloscope but no glitch are found. I saw only a voltage dip of 100 mV. I place a small capacitor on the GPI input and I don't see the voltage dip but the problem still exist. I measure also the sequencer power but no voltage dips are found.
This problem occurs only when an open-drain output (pin 11) is pulled low by an external device.
Next I make an other GPI dependence (only pin 20) and the problem doesn't appear!
Any idea?