This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Smallest-size Li-ion 4-cell (series) charging solution?

Other Parts Discussed in Thread: BQ24725A, BQ24610, BQ24725

I'm hoping for some help in selecting the smallest-size solution for charging a series 4-cell Li-ion battery pack.  We need to both run the system and charge the batteries when the AC adapter is plugged in.  The system load current could be up to 3 A, but the charge current isn't critical because it's okay to take hours to charge.  We could charge at a fraction of an amp if that helps.  We can size the AC adapter as needed, both for its voltage and its current rating.  We have a microcontroller in the system, but we want to minimize how much charger management it needs to do.  So, I'm looking for simplicity and, as I said before, the smallest footprint possible.  I've been reviewing the available TI parts, and the bq24725A has potential, but I can't help wondering if there's a solution which is simpler.

Thanks,

Scott