This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Multiple cells (series/parallel) battery charger?

Hello all,

  To maximize the stored energy for my application, I am using three battery packs (PDA-284LI). in parallel.  Each pack has 2200 mAh capacity at 3.7V.  I think it consists of two 1100 mAh cells in series. I am bound to a certain size and form factor so that is why I chose these packs.

I am finding solutions for single cells or multiple cells in series but not for a series/parallel combination.

 Is there a clean solution that will help me charge the batteries in the setup that I have?

Thank you for your time and effort.

Amer