I am designing an indoor LED lamp and consider using the TLC5970 driver.
The LEDs can sink 30mA each, so my plan was to use 3 in series and 4 in parallel for each output.
Has someone already done a setup using multiple parallel LEDs per output on the TLC5970 ?
I think it should work fine, however in the event of a LED failure, the LEDs in parallel might be damaged ?
In my understanding of the datasheet, the TLC5970 will attempt to raise the Voltage of its own DC/DC converter output, to keep the current level on the output ports, which may lead to over-current on the other LEDs.