This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DC/DC Buck Converter that can sink Current

Other Parts Discussed in Thread: TPS54310, TPS54352, TPS54350, TPS54320, TPS54550

Hi all,

I am looking for a buck converter that can sink current with the following requirements.

This will be used as a simulated battery.

Input:  5V -> 16V
Output: 3V -> 12V
Output Voltage needs to be adjustable

Current Source: 1000mA
Current Sink:   1000mA

I found the TPS54310, however the output voltage is to low.

I found TPS54352, but these seems to only be fixed output voltages, and the current is a bit too low.


Any tips on a potential part number would be great.