The standard procedure is to discharge the battery and let it rest for 5 hours. What happens if I discharge the battery down to the level where the Z95 shuts off. I insert the battery into the charger and it will wake up. How does that effect the learn cycle? Will the 5hrs rest start at wakeup?
I have a battery that stays at 4% error when it is running in my cycler. The cycler waits for just 2 hr between charge and discharge cycle.
Mike