This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

High Vin LED driver

 Does TI have new product roadmap that can meet below SPEC for automotive lighting?

 

Customer: SCI (TW, Tainan)

Application: Automotive lighting

Topology: Buck-Boost

Competition device: HV9910 ($ 18TWD). It already M/P

Vin range: 9V to 36Vdc

Vout Range: 7.2V(2 LED) or 10.8V (3 LED)

LED topoloty:2S2P or 3S2P

LED watts: 3W/pcs

Voltage stress Test item: 90V with 0.4S (SCI internal qualification process)

 

Original, we promoted and DIN the LM342x series to customer side. But it was fail to test item of voltage stress (90V with 0.4S, reliability test).

So do you have any idea to solve this? Or other suggestion of suited device?

 Thank, Brian