Got another question regarding the TPS40210 and I couldn't find the answer using the search function.
Does the PowerPad have to be grounded or can it be soldered to a logic level network with wide traces (for heat dissipation)? Specifically, in my application, I could substantially improve the layout if I soldered the power pad to the network of traces that control the EN/DIS pin on the TPS40210.
Additionally, if a different method of heat removal was provided, would it need to be grounded? E.g., on a prototype board that was to be hand soldered, could I put a dab of thermal compound between the copper trace and the PowerPad and assemble it that way? Or perhaps a dab of thermal compound and a heatsink above it?
Thanks!