Sir:
I use pth08t240w in my board, and the sechmetic is in PIC(1). In my design, I use the TurboTrans Technology, and I choose the input capacitor Ci and output capacitor as follow:
type |
Rated Volt |
Capacitance |
ESR(m ohm) |
||
Ci |
6TPF470MAH |
6.3 |
470uF |
10 |
|
Co |
4TPF680MAH |
4 |
680uF |
10 |
But the input and output of pth08t240w is with much more noise than that was described on the datasheet. The output of pth08t240w has a Vo ripple more than of 70mv, while the datasheet saied it should be about 10mv. The test of pth08t240w input and output is in PIC(2) in below.
Is there something wrong for my using with pth08t240w? Why this DC-DC work so terrible in my board?
PIC(1) the schematic of pth08t240w in my design
PIC(2) the output and input voltage of pth08t240w tested with oscilloscope. The yellow signal is the output voltage of 1.0v, and the red signal is the input voltage of 5.0v.