I've got a couple questions around the BQ25050/BQ25060 parts.
I am unclear as to the operation on "OUT". From the datasheet I can see that it will be greater than 3.4V when there is an input. It also mentions that Vout is regulated to 3.5V.
So what I am wondering is this:
If there is no input voltage, what is the value of Vout? Is it regulated to 3.5V from the Battery?
What is the max current of the OUT when input voltage is present? Can I put a 3A load on the OUT pin, a 30mA load on the LDO and charge the battery?
Thanks