This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL494 application

Other Parts Discussed in Thread: TL494

In "Application Report. SLVA001E–December 2003–Revised September 2011" , figure 35, and in several other documents with TL494 applications the reference input to pin 2 is divided by 2. What is the reason to do so ?. As I understand this reduces the loopgain by 50% plus it requires an additional resistor, so where is the advantage?  

I would appreciate an explanation since in my apllication I have fed the full 5Volt reference into pin 2 and the circuit works reasonable well, although the switching frequency and duty cycle are not stable in all conditions between minimum and maximum load (battery charger).

  • Arie,

    The useful range of the error amp output is between 0V and 3V. Keeping the common mode input voltage close to the output voltage lowers the average current and voltage drop on resistor R5 (figure 35). It also ensures a good common mode voltage when VCC is at minimum, 7V.