How much current does the TPS65930 draw when only the RTC is running. I am trying to size a coin battery for this purpose?
Thanks,
Steve
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How much current does the TPS65930 draw when only the RTC is running. I am trying to size a coin battery for this purpose?
Thanks,
Steve
Steve,
This parameter is specified in TPS65930 Data Manual page 47(backup current , 2.25uA)
I sized my battery using the 2.25uA backup current specified on page 47 of TPS65930 Data Manual. I'm getting reports from the field of dead batteries much sooner than expected. I'm using CR1220 coin cell battery that has 35mAh capacity. I am measuring a current draw from the backup battery of 8.9uA, almost 4 times what the datasheet states.
A few notes:
1. Inserting the battery into a board that is powered down (Vbat = 0V), there is no significant current draw from the backup battery (Vbackup=3.2V, @0uA).
2. Power up the board (Vbat = 4.2V) and there is no significant current draw from the backup battery (Vbackup=3.2V, @0uA).
3. Power down the board (Vbat =0V) and the backup current spikes to 50uA for a second or less and settles at 8.9uA.
4. Only time I measure 2.25uA current draw from backup battery is when I remove the backup battery (Vbackup=not present) while powered down (Vbat=0), short BKBAT pin to ground, and reinstall the battery (Vbackup =3.2V, @2.25uA) while powered down (Vbat=0). At this point, the time and date are lost so if the current is being used to power RTC, it's not the correct time and date.
Please help.
Daven
Hi Daven,
You have to set CK32K_LOWPWR_EN=1 to enable the 32KHz clock low power mode and decrease the backup consumption to 2.25uA max(1.7uA typical).
regards,
Alexis