Dear Sir or Madam
Data-sheet for UCC38503 does not contain tolerance for the value of PFCOVP threshold level.
It only has a value of 8V on Block Diagram (page 8). In Pin Assignment for “OVP/ENABL”, it says that “A window comparator input which disable the PFC output driver if the boost output is 6.67% above nominal”. Could you, please provide tolerance for this parameter.