Hi,
Kindly suggest a suitable device for the following specs:-
Input = 6V to 32VDC
Output = 5V at 2.5 Amps, with Load dump protection upto 150V.
Protections reqd = Over current and Short circuit
Regards
Atul Bhakay
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Kindly suggest a suitable device for the following specs:-
Input = 6V to 32VDC
Output = 5V at 2.5 Amps, with Load dump protection upto 150V.
Protections reqd = Over current and Short circuit
Regards
Atul Bhakay
Hi Atul.
How long it is this load dump?
I don't think there are availables IC able to work with these high voltages.
You've to limit your spike in other ways and then regulate with a "normal" IC...
If load dump is not so long you can look for tranzorbs...
On 24V ECU, we usually put a tranzorb on the DC link and the load dump is in the range 200-400ms...
Bye
Paolo