I plan to use this regulator evm to step up the voltage from a BQ Tesla wireless power receiver supplying 5V@1A to about 14.6V in order to charge a sealed lead acid battery, at a slow charge rate of about 300mA. I have reviewed the schematics of the eval board and they match my design almost identically except for the fixed output voltage of 12V. I am planning to change R2 of the feedback divider with a 39kOhm resistor and a 10kOhm trim pot in series in order to achieve 15Volts. I understand that replacing R1 would be ideal but R2 will be much easier for me and if my estimates are correct it would only step up feedback current by about 100uA. I believe this would just be a loss in efficiency and will be dealt with in the migration from prototype status. I was just wondering if you had any advice on this.
Thank You in advance
Shane