This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need Charger IC advices ...

Hello,

I'm trying to design a 9 cell li-po battery management system which requires a charger with specifications for each cell such as written down bellow :

 1. Rated Capacity : 76,5 Ah

2. Max Charge Current: 225 A

Do have any charger IC's which will charge these each cells with the required specifications writtin as...

  Fatih