I can put R1=909k and R2=576k in REG104A for Vout=3.3V?
The REG104A work correctly with high value in the resistors?
Regards,
Julian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I can put R1=909k and R2=576k in REG104A for Vout=3.3V?
The REG104A work correctly with high value in the resistors?
Regards,
Julian
Hi Hugo,
The leakage current from the feedback (adj) pin may introduce accuracy errors when using higher value resistors (see figure 2 and note the variation is I_adj shown in the graph in the Typical Characteristics section of the data sheet). Please take note of esr requirements for the output capacitor (if needed). And please add a place holder for Cfb.
Regards
Bill