Hello: I have an inquiry from my customer:
>>>>>> I have the LM5019ISOEVAL EVM. I'd like to know if webench supports running the reference design schematic (using a coupled inductor as an isolation transformer like what is done on the reference design)? I would like to use the coilcraft LPD3015 series inductor if possible (http://www.coilcraft.com/lpd3015.cfm). We need to be able to fit this circuit under 2.8mm tall. The LM5019 uses a LPD5030, which is 3.0mm tall (too tall). I would like to put the LPD3015 series inductor into the webench simulation of the LM5019 ref design, but I can't find that isolated supply reference supply in webench. Any issues with dropping the LPD3015 coupled inductor into the LM5019 ref design circuit in place of the LPD5030? >>>>>>>
EAU is 5k. Thanks. George Biner, FAE Arrow LA