I'm usign TPS61220 on a 2-battery cell powered device. So, input voltage is 3.3V throug 1.8V. I need an output of 2.8V, 60mA.
Since the part will be working with Vin > Vout for a while (2.8V through 3.3V), I expect no regulation above the output. My question, is there any risk with the part being damaged during that period?
Is there any alternative part/solution to the above?
Hubert