Hi,
I would like to know the max frequency of the output driver(Ho1, Ho2,Lo1,Lo2) of LM5045.
Since the frequency of the oscillator is 2MHz, does it mean that the max frequency of the output driver(Ho1, Ho2,Lo1,Lo2) of LM5045 is only 1MHz so that the output of simplest full bridge DC-AC converter can only work at 1MHz?
If it is so, are there any Ti products can generate a 1-2MHz square wave with 40V Vpp?
Thanks for your time