Hai
I would like to design a full bridge smps using UC3875 IC, for a 24V 40A smps. I would like to use transformer coupling for gate driven. But in the trail version the the gate wave forms have glitches and the mosfet getting over heated when i use a feed back control from the output. the ckt i used for this is attached with this.
with Regards
Emil Jose3755.3875 apps.pdf