Hi,
The LM5118 datasheet states the following: If the EN pin is below 0.5V, the regulator will be in a low power state drawing less than 10 µA from VIN. EN must be raised above 3V for normal operation.
The exact same data can be found in the Electrical Characteristics (EN INPUT)
However, it appears that the EN Input High Threshold is much lower in my circuit (around 1.7V). Can it be specific to the chip I am using or is there an error in the datasheet?
FYI, I use a resistor voltage divider on the EN pin in combination with another resistor voltage divider on the UVLO pin to provide a wide input voltage turn-on/turn-off window. E.g. Turns on @ Vin=20V, and locks on till Vin drops below 12V.