I test UCC27322TDGKREP gate driver with function generator input and want to let it operate at 13.56Mhz to drive 650V CoolMos with Ciss= 5nF, which it need very High gate power
after the test I can only increase the frequency to 1.2Mhz and the IC start to work nonfunctional, if I increase frequency more , the IC will break down.
So I found there's another Power pad package UCC27322DGN package which could operate at 3W power dissipation, rather than P package 350mW
So if I want to achieve 13.56Mhz is it Possible to use that DGN package to realize?