This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About BQ25504 several question

Other Parts Discussed in Thread: BQ25504

Hi

I have question for about BQ25504 Data sheet Fig 22 means

Question

No1. About Fig 22  each mean

a)   Fig .22     0.2V  ~ 1.4V (Chip Enable)

    What dose mean Chip Enable? and Chip enable purpose??

b)  Fig.22      1.4V ~ 1.8V  ( Charger Enable)

    What dose mean Charger Enable and purpose??

c) Fig.22       1.8V  ~ 2.2V ( Under Voltage)

   What dose mean under voltage  and what happen??

d)  Fig 22     under voltage (2.2V)   ~ +hyst (internal)  

  Q :  What purpose  "under voltage +hyst"  and  what happen?  

e) Fig 22    undervoltage +hyst  ~ over voltage - hyst  

    Q :  Wgat purpose  "over voltage -hyst"  and purpose?

 f) Fig22   over voltage - hyst  ~ over voltage

    Q:  What purpose  "over voltage ? " and happen?

g)  Fig22  over voltage ~ device absolute

   Q:  What purpose this during over voltage and device absolute and purpose? 

 

No2        Q :  Wtat diffrence  "Cold start " and  "Boost Charger ON" ??

No3.       Q:  if  we set to  Over Voltage =3.3V  and Under Voltage=2.2.

                      Which is start   rechaege Voltage  after dis charge ??

No4.      Q:  About  BAT_OK and OK_PROG, OK_HYST Pin.

                  If not use these pin  which is correct?    Open  or  Pull UP/ Down??

 

Could you answer to us??

Thanks and Regard

Jasper