Hello
How is it possible to completely disable WLED driver, or can I just leave pin floating (L4,FB_WLED, ISINK1/2, ISET1/2)
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
How is it possible to completely disable WLED driver, or can I just leave pin floating (L4,FB_WLED, ISINK1/2, ISET1/2)
Thank you!
The WLED driver is off by default. The only way to turn it on is to use the ISINK_EN bit in register 0x07. As long as that bit stays low, the WLED driver will be off.
Regarding the pins:
L4, FB_WLED, ISET1, ISET2 -- leave these floating
ISINK1, ISINK2 -- connect to ground