Hello,
I'm posting this on behalf of my customer:
Customer is looking to use LM5117 and sees it has an analog current monitor to track current to the inductor. Is there a way to use this function to limit inrush current coming into the LM5117? They would need to limit to 1.2A max? If not, is there another DC/DC product that has in rush protection built-in that can support a wide input from 10V-52V like the LM5117?
Thanks,
Tom