Hi,
One of my customers in Australia is looking for a Single DC-DC Converter which can provide the following:
Vin: 6.6V-7.2V, Vout1: 5V, Iout1: 2A
Vin: 11V-14V, Vout2: 7.2V, Iout2: 1A
Is there any suitable single part that can help or will the solution need two DC-DC regulators. Please help me with the part number.