We got this issue with approx. 15% of our new manufactured boards, which are unprogrammed. What we already know:
Supply voltages present: VDD1 & VDD2 = 1V2, VIO = 1V8, VRTC.OUT = 1V5. VBAT is ~ 3V8
26 MHz Clock present at PMU 2-3 ms after oscillator is powered, looped from PMU (32CLKOUT) to AM3703 sys_Xtalin (also present there)
32.768 kHz RTC-Clock present at PMU, looped from PMU (HFCLKOUT) to AM3703 sys_32k (also present there)
CLKREQ from AM3703 to PMU is HIGH (not active)
PMU NRESWARM & NRESPWRON are HIGH (not in reset)
That means power sequencing as in datasheet chapter 6.5.4.2 is complete & fine
But VDAC.OUT & VPPL2.OUT keep low as INT1 from PMU to AM3703 (SYS_NIRQ) does
We have no external RTC, no USB present, no charger present,
Boot Mode is set to Master (Boot1 with 10k pull-down o GND, Boot0 with 10k pull-up to VBAT (3V8))
Any hint is welcome. What causes INT1 keeping permanent low?
Thomas