I have designed a battery board with the bq3060. I have designed many battery gas gauge boards in the past and I don't believe I have a faulty schematic. I have verified that the connection from the pin to the resistor isn't shorted to any other nets.
On the bqEval software, the FET Status register indicates both the CHG and DSG bits are set but, the voltage on the 5.1k resistor from the gate to the IC is at the battery voltage. The pull-up resistor, gate-to-source, is 3.01M, same as on the bq3060 Eval Board.
I have replaced the bq3060 IC on the board to be certain that wasn't the problem.
I'm attaching a screen-shot of the bqEval software.