Hi. I'm designing a type 2 PoE PD. I'm thinking about using TPS23756, The system limitations are:
-12v Output at 1.5 A.
-Auxiliary input range: 12-18 VDC.
- Efficiency: > 85%
-Auxiliary has the highest priority.
Could you please help me with a circuit schematic and BOM. and if there is a design example shows how to determine the values according to the system requirements it would be better because i might need other designs for other power levels.
Thank You