Hai Support,
I am using BQ24170 in my design and trying to power it up with the 12V input for the single cell configuration. I expect that the system side output to be regulated to 4.2V when I use single cell configuration. But I am seeing that 12V is bypassed to system side without any regulation. I am able to see 4.2V on the battery output but the expected 4.2V is not coming on the system side from the ACFET and REVFET mosfet's. Can somebody please help to check what could be problem here.
Regards,
Erfan