Hello,
I'm using the LM3409 Demonstration Board. I'm having a problem pulsing LEDs at low frequencies. I'm eventually trying to enable the LEDs with a 60 Hz PWM at 2% duty cycle.
I've tried various low frequencies and whenever the off-time (low part of duty cycle, not switching frequency) is greater than ~11 ms, there is a delay and no constant current to the LEDs. I've pored over the datasheet, but I can only find information related to higher PWM frequencies.
What would possibly cause this problem? The only information I see is related to the off-time of the switching frequency for the peak current detection / regulation.
Thanks