This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tps65950 push button

Other Parts Discussed in Thread: TPS65950

hello ,

what register and what bit to check or it will be set in tps65950 ic when push button is pressed for 8sec

thanks

  •  

    Hello,

    You will find registers information in TRM document.

    regarding teh 8s PWRON button press, this is page 289, STS_BOOT register.

    http://www.ti.com/litv/pdf/swcu050g

     

    regards

    Alexis

  • hi alexis,

    Thanks for your guidance, but my problem is when is press the push button momentarily the device will restart and if i press hold that button for 8sec or more, then also it will restart, but i want device to restart only when the button is pressed for more than 5sec. I checked for the PWRON_8S bit in STS_BOOT it is not at all setting even if i press for 8sec or more , for this bit to set what all configuration i have to make and in what all areas i have to look ( like schematic or so ) and i want to know how this 8sec time is counted by tps65950 plz explain in detail.

    Thanks

    regards

    ram m h


  • Short press on PWRON button(more than 30ms and shorter than 8s) only generate an interrupt.

    There are multiple reason to have the PMIC shutting down before the 8s:

    1) on PWRON press, software shut down PMIC

    2) PWRON has been configured as a swiutch off event--> please check P1_SW_EVENTS register value

    3) PMIC has been configured in slave mode--> please check CFG_BOOT register value and check how the BOOT0 and BOOT1 pin are connected on the pcb

     

     

    regardds

    Alexis

  • k thank you alexis i will go through it and come back to you

    regards,

    ram m h