hi,
questions regarding BQ24278:
- When AC adapter is connected (lets say 5V) what is the voltage at SYS/SW pin (out pin connect to the load)?
- Which voltage is recommended to supply for high efficiency and minimum heat dissipation?
- What are the consequences if I connect load directly to the battery? this load will operate only at backup, when AC adapter is not connected.
- when AC adapter connect the total current consumption is about 1.6A (not include battery charging) at 3.3V (i use buck-boost switcher to reduce voltage). one of the feature is GPRS module(GE910). its average current consumption is 220mA, but has 2A current picks. can this influence on the output supply both when adapter is connect or battery discharge?