we are selecting a pfc front end circuit to our volt-hertz 3 phase 3,500W ac drive. the input is NOT universal but 240VAC +/- 10% single phase, and we would like an output of around 385VDC. Could someone recommend the best topology for this, single, interleaved or bridgeless. If interleaved is the way to go, could you recommend a boosting inductor value (along with current handling capacity) and a switching frequency that would work? The design spread sheet that TI offers is for universal input, down to 85VAC, which puts an extra burden on the design. Ideally, if someone could direct me to a successful design of such a circuit it would be very appreciated. thank you.