Hi,
I wonder if the input voltage exceeds the maximum value in the datasheet(5.5V), what will happen? There will be a short circuit or open circuit, or even cause permanent damage to the chip?
Thank you very much!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I wonder if the input voltage exceeds the maximum value in the datasheet(5.5V), what will happen? There will be a short circuit or open circuit, or even cause permanent damage to the chip?
Thank you very much!
We can't say for sure what will happen, but any of the above might happen on a given IC. Operating with too high of a voltage might overstress the chip. Thus, operating outside of the recommended operating conditions is not recommended. We have the TPS63060 for higher input voltages.