Hello,
I'm looking for any information on specific failure data on CSD25302 and CSD16301. I would like to know if these MOSFETs could fail having a D-S resistance of around 5 to 10 ohms and able to conduct 3 to 7A continuously, while damaged. I know that there is some information about Reliability Data from the product folder but any further information would be greatly appreciated!
Any additional failure data on these two parts would also be greatly appeciated!
Regards,
Rachel