With regard to the TPS65910A3 it seems that this PMIC supports charging of Li-Ion batteries. Is there any kind of overcharging protection built into the chip?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
With regard to the TPS65910A3 it seems that this PMIC supports charging of Li-Ion batteries. Is there any kind of overcharging protection built into the chip?
Hello Mike,
There is a backup battery charger, but this is not intended for LiIon, more like it's for a supercap.
BBSEL Back up battery charge voltage selection: RW 0x0
BBSEL[1:0] = 00 : 3.0 V
BBSEL[1:0] = 01 : 2.52 V
BBSEL[1:0] = 10 : 3.15 V
BBSEL[1:0] = 11 : VBAT
There are 4 settings, none of which represent a Li-Ion 4.2V charge profile.
There is not a Li-Ion charger in this device.