Hello all, I am using the bq3055 Li-Ion battery pack manager for a school project and one of its features is continuously monitoring current so it can use the method of coulomb counting to monitor the capacity of the battery. As I was reading the datasheet for the bq3055 to try and figure out what exactly it meant by "continuously" monitoring the current I found on page 17 in the 'Charge and Discharge Counting' section it states "The bq3055 continuously integrates the signal over time, using an internal counter. The fundamental rate of the counter is 0.65 nVh."
As an EE student, I have never seen the unit nVh before. Can someone please explain to me what it means when it sates that the rate of the counter is 0.65 nVh?
Thank you very much in advance!