According to the Power Management guide (http://www.ti.com/litv/pdf/slvt145l) LM3448 is intend to use in application below 8W.
From another side in the datasheet (http://www.ti.com/litv/pdf/snosb51b) there is no direct parameter which prove this. Indeed we have integrated FET with breakdown voltage 600V and maximum peak current 1.2A thus even if we will use the FET at values equal 75% we obtain FET power capability 400W.
Thus I guess the main limited factor will be power dissipation of the package but this parameters is not mention in the datasheet.
Could somebody clarify what parameter exactly limit output power of the LM3448 for values below 8W?
best regards,
Oleksiy