Hello, we have successfully implemented a BMS with 18 BQ76PL536A devices monitoring 102s1p 20Ahr LiFePO4 cells. Two times it happened that the cells corresponding to a given BQ IC got discharged below 2.0V in less than 24hrs.
A first guess was that the bleeding resistors were unintentionally switched on; however they are set to limit the current to 100mA therefore it is not possible to fully discharge the cells in one day.
The same behavior was seen on the testbench one or two times using a '536EVM with 18s1p 1.1Ahr LiFePO4 cells. Overnight one section of 6 cells was discharged below 2.0V.
In our battery the '536s are hot plugged to the battery, the cell voltages are applied in a random order to the '536 terminals. I remember reading some information that this is not a problem for the '536.
We are not able to reproduce the problem nor explain the reason for which the cells get discharged, I wonder if somebody has faced this problem or there are any ideas. Thank you.