This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AC-DC Reference solution needed

Need a solution for the below specifications.

Is there a reference design available for the below AC-DC Application

90-275V input desirable, 190-265 mandatory.

                85%+ efficiency.

                13.75V output (+/- 100mV) – 6 cell SLA battery float charge voltage.

~8A would be desirable – That’s actually 110W, but 100 would do if the extra 10W pushed us over a price or reliability precipice.

                Ability to reduce output voltage under analog input control 11V-13.75V

                0-55 degrees C, 85% non-condensing

                CE, C-Tick and A-Tick compatible.

                ROHS.

 

                No Fans

                Economical to manufacture, transformer supply identified and priced.