V in = 12 - 24 V, V_out = 5.1V, I_out = 5A, V_EN = 0 or 3.3V (CMOS Logic output), C_out = 68uF.
As LOAD post motherboard connected +5 V 15W, С_in ~ 820 uF.
If V_in set 22V, V_EN set 3.3V - LM3150 have start and after 5-6 ms - off and have not restart.
If V_EN set 0 and then set 3.3 V, the process is repeated.
Questions:
How to include current limit load 10 to 15 ms for the LM3150?
How to improve the situation for the LM3150?
Thanks in advance,
Lo