I am using SwitcherPro to design a pretty basic 180-30V to 3.3V buck converter with a max output of 1.375A. I assume the loop plot that SwitcherPro generates uses data relative to a 1.375A output, but in my design that is a worst-case output (multiple fault conditions). The circuit should be operating closer to 400 mA most of the time. Does the loop plot still apply at that load?