Hello!
I'm a student from China and I need to determine whether it is suitable to use ADS1298 to measure EEG.After I read the manufacture's datasheets.I found it's CMRR is -115dB,I wonder whether its definition here is 20log(Acm/Ad).Then,from datasheets I know that the referred input noise is 4 uVpp(150Hz BW,G=6).But in the table 6,when the gain is 6,the BW is 64kHz respectively.I don't know why.
Thanks.