Other Parts Discussed in Thread: TLC5927
Hello,
I have a question regarding the LED driver TLC5927. Currently I am designing a simple circuit using 3 TLC5927 and a PIC microcontroller. I have some questions regarding the connection in cascade an the dimensioning of R-Ext.
1. Are there any problems sharing the 3 CLK on one pin at the microcontroller?
2. Same goes for sharing the LE(ED1) and /OE(ED2)? Are there any additional Pullup/Pulldowns required?
In result I only need 5 Pins for controlling 3 TLC5927 with my microcontroller (common CLK, LE(ED1) and /OE(ED2) plus SDI and SDO)?
3. Calculating the R-Ext: I am trying to controll RGB LEDs (16pcs -> one TLC per color) using Vdd = +5V. The datashee says red max. 2,6V / green max. 3,6V / blue max. 3,6V. The max. current for each color is rated at 10mA. So how do I calculate R-Ext for each TLC (color) in respect to the max. voltage an Vdd. Unfortunately I did not understand the calculation in the datashee concerning this. Say that I want to have the 10mA as max gain.
Thank you for your help in advance
Greetings from Germany