On page 19 of the TPS6213x datasheet you give a list of recommended inductors, some of which are rated BELOW the static current limit of 4.9A max. If I use one of the inductors, lets say the VLC5045T-3R3N from TDK (rated 3.3nH at 4A), wouldn't there be a chance, at full load, that the inductor wold be overloaded?
I am using a 3.3nH, 4A inductor and am wondering if I need to switch to one with at least a 4.9A current limit? But you suggest a 4A one in the datasheet.
Thanks,
-Aaron Weiss
SparkFun Electronics